2021-11-05 9:11 AM
Also how to internally connect the input trigger to two simultaneous one-pulse generators.
2021-11-05 9:58 AM
There really isn't an internal connectivity fabric
The TIM can cross their own CH1/CH2 and CH3/CH4 channels (direct/in-direct), and there is some input/output triggering plumbing which connect specific TIM/CH between each other.
The AF MUX fabric really only allows for a single peripheral connection to a pin.
2021-11-08 3:31 PM
is this the correct set up for a one-pulse?does not seem to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.