2025-05-02 10:24 AM - edited 2025-05-02 10:27 AM
I've just brought the stm32h573i-dk dev board and what to become familiar with Threadx and USBx. I have a uni project coming up that I would like to use the board as a msc device but struggling to get the board to enumerate with the PC. I have tried to get majority of the USBx reference designs up and running. They compile fine but nothing happens when I connect the board to a PC on cn17 ( the non stl-link usb). Is there anything I'm doing wrong to get it up and running . Is there something I need to enable to for the USB port to work?
I also have a couple of u5 and h5 nucleo boards I would also like to get up and running With various forms of USB Once I have the discovery board working. Any pointers would be greatly welcome. Thanks
Solved! Go to Solution.
2025-05-12 2:50 PM
Hi FBL,
I have just revisited looking at the USBx examples but used a different USBc cable and all examples
work. It looks like a power only cable had got mixed in with the cables.
2025-05-05 2:38 AM
Hi @Sidewinder
Did you insert SD card before application is started?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-12 2:50 PM
Hi FBL,
I have just revisited looking at the USBx examples but used a different USBc cable and all examples
work. It looks like a power only cable had got mixed in with the cables.
2025-12-08 10:10 AM
I’m having the same issue. The STM32H573I-DK example USBPD_SRC_UX_Host_MSC compiles normally, but when I plug a USB flash drive into the board, nothing happens. The board doesn’t detect or respond to the device.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.