2024-06-18 1:01 AM - last edited on 2024-06-24 3:01 AM by FBL
I have tried setup STM32G071 Sink port and connected with Apple 140w. I want to request 140W but it's seem STM32 not yet supported EPR mode in PD core. Do you have any examples for EPR in STM32?
Solved! Go to Solution.
2024-06-25 1:25 AM
Hello,
As of today STM32 support SPR and has to be used with TCPP0x.
Our next version TCPPE with an update software for STM32 will be compliant with 140 W (EPR) but it is not available today.
Regards
2024-06-18 6:06 AM
Hi @H V N D
You have already got your answer, I think here.
Solved: USB PD sink - STMicroelectronics Community
Firmware is already supported in TCPP stack. Unfortunately, we cannot predict the release date of full solution including new HW shields.
Thank you for your understanding.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-18 3:32 PM
Hi FBL,
Will the full solution also include examples of 140W SRC support?
2024-06-18 3:42 PM
2024-06-19 5:14 AM
Hello,
The current products (TCPP0x + STM32) are able to manage up to 100 W (SPR mode). The next solution (TCPPEx + STM32) will be able to manage up to 240 W (EPR mode). In your case the suitable product will be TCPPE2.
Regards.
Philippe
2024-06-19 4:57 PM
Hi,
Thanks for the update @Philippe RABIER
We have developed our own 140W capable power bank using the STM32G071. 15-100W SRC has been implemented and we're about to add support for 140W. Are there any code examples or documentation for implementing 140W EPR SRC support?
2024-06-25 12:32 AM - edited 2024-06-25 12:54 AM
Hi @Philippe RABIER , @FBL
Any update on this? Is this something our FAE can perhaps help better answer?
2024-06-25 1:25 AM
Hello,
As of today STM32 support SPR and has to be used with TCPP0x.
Our next version TCPPE with an update software for STM32 will be compliant with 140 W (EPR) but it is not available today.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.