2015-04-08 8:04 PM
I a writing a USB HID program for STM32F107, but when i look at the USB HID library from STM, i am so confused and cannot understand the library for my own modification, such as where is the descriptor, how its value is set...
Anyone can suggest me any docs for this or sample project. Thanks very much2015-04-09 4:05 AM
Hi,
Look at UM0424 available in this page: http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF258157.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-04-13 2:57 AM
#if defined(STM32L1XX_MD) || defined(STM32L1XX_HD)|| defined(STM32L1XX_MD_PLUS)|| defined(STM32F37X)|| defined(STM32F30X)
/* Enable the SYSCFG module clock (used for the USB disconnect feature) */RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);#endif /* STM32L1XX_XD */ /* Set all the GPIOs to AIN *************************************************/// Configures all IOs as AIN to reduce the power consumption.//#if !defined(STM32L1XX_MD) && !defined(STM32L1XX_HD) && !defined(STM32L1XX_MD_PLUS)&& !defined(STM32F37X) && !defined(STM32F30X)GPIO_AINConfig();#endif /* STM32L1XX_XD */ #if defined(STM32F37X) || defined(STM32F30X) /* Enable the USB disconnect GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIO_DISCONNECT, ENABLE);
/*Set PA11,12 as IN - USB_DM,DP*/
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);/*SET PA11,12 for USB: USB_DM,DP*/
GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_14); GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_14);1. I dont understand about USB disconnect feature in the bold lines. Could you explain to me why we need USB Disconnect?]2. And the last two red lines: IN- USB_DM.DP and USB_DM,DP. Are they different? Please explain? Thanks very much!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.