2015-06-18 3:09 AM
Hello, i'm trying to develop an usb composite device(MSC+HID classes) on STM32F407 using the USB Device Library that comes with the STM32Cube.
Basically what i've done is importing in import already working codes for standalone MSC and HID classes and create a new layer on the usb calls stack. I've declared a new USBD_ClassTypeDef USBD_COMPOSITE = { USBD_Composite_Init, USBD_Composite_DeInit, USBD_Composite_Setup, NULL, /*EP0_TxSent*/ NULL, /*EP0_RxReady*/ USBD_Composite_DataIn, /*DataIn*/ USBD_Composite_DataOut, /*DataOut*/ NULL, /*SOF */ NULL, NULL, NULL, USBD_Composite_GetCfgDesc, NULL, NULL, }; where each composite function pointer looks like this: static uint8_t USBD_Composite_Init (USBD_HandleTypeDef *pdev, uint8_t cfgidx){ uint8_t ret = 0; pdev->pClassData = USBD_malloc(sizeof (USBD_HID_HandleTypeDef)+sizeof (USBD_MSC_BOT_HandleTypeDef)); if(pdev->pClassData == NULL) { ret = 1; } else { (USBD_HID_CLASS)->Init(pdev, cfgidx); (USBD_MSC_CLASS)->Init(pdev, cfgidx); ret = 0; } return ret; } In the main the code to start the component looks like: USBD_Init(&USBD_Device, &Composite_Desc, 0); USBD_RegisterClass(&USBD_Device, &USBD_COMPOSITE); USBD_MSC_RegisterStorage(&USBD_Device, &USBD_MSC_F4Memory_fops); USBD_Start(&USBD_Device); As u can see pointers to HID and MSC class functions are not called explictly by the Core functions but accessed trought the struct USBD_COMPOSITE that handle the redirects. Analizying the behaviour of the component via USBlyzer what happen is Babbled Error on a Get Descriptor request my code is able to handle. Reading the USB 2.0 specification this error is caused by bus activity from the device after the EOF that triggers the hub to disconnect the port from the host. Does anyone have any suggestion on the nature/cause of this error and how could be possible to solve it? PS: I'm uploading the eclipse project and the link will be avaible as soonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.