2017-06-20 10:06 PM
Hi,
I'm using Nucleo F207ZG , I'm trying to send the message using xQueueSend from CDC_Receive function but the following i cant because of priority level ,
Program received signal SIGINT, Interrupt.
0x080030dc in vPortValidateInterruptPriority () at ../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM3/port.c:709configASSERT( ucCurrentPriority >= ucMaxSysCallPriority );Any suggestion ?
-Thanks & Regards
K.Manikandan
2017-06-21 12:54 PM
If you look in the source code at that point there is a long comment that, I think, gives you the answer you are looking for. Reproduced here (cut out of the source code at the point you are highlighting yourself). Not the references to further information on the FreeRTOS.org website:
/* The following assertion will fail if a service routine (ISR) for
an interrupt that has been assigned a priority above configMAX_SYSCALL_INTERRUPT_PRIORITY calls an ISR safe FreeRTOS API function. ISR safe FreeRTOS API functions must *only* be called from interrupts that have been assigned a priority at or below configMAX_SYSCALL_INTERRUPT_PRIORITY.Numerically low interrupt priority numbers represent logically high
interrupt priorities, therefore the priority of the interrupt must be set to a value equal to or numerically *higher* than configMAX_SYSCALL_INTERRUPT_PRIORITY.Interrupts that use the FreeRTOS API must not be left at their
default priority of zero as that is the highest possible priority, which is guaranteed to be above configMAX_SYSCALL_INTERRUPT_PRIORITY, and therefore also guaranteed to be invalid.FreeRTOS maintains separate thread and ISR API functions to ensure
interrupt entry is as fast and simple as possible.The following links provide detailed information:
*/We’re moving the ST Community to a new platform to give you a better and more reliable community experience.