2018-05-11 7:01 PM
hello every body. I'm new here. I've just started learning STM32F373 with STM32F373VCT6. I use CMSIS to configure UART1. that seems there're no any error with my code. But when I use PL2303 to convert serial-usb for connecting with PC. I dont receive anything. Here is my code. Can anyone help me to find your mistake. Thanks in advanced
/*==============================================*/
/* Includes ------------------------------------------------------------------*/
#include 'stm32f37x.h'#include'main.h'uint8_t ledVal = 0; static __IO uint32_t TimingDelay;/* Private typedef -----------------------------------------------------------*//* Private define ------------------------------------------------------------*/#define BSRR_VAL 0x0003/* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*/GPIO_InitTypeDef GPIO_InitStructure;/* Private function prototypes -----------------------------------------------*/uint8_t SendChar (uint8_t ch);void GPIO_Config(void);void USART1_Config(void);uint8_t GetChar (void);int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f37x.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f37x.c file */ //SystemInit(); /* GPIOC Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);/* Configure PC0 and PC1 in output pushpull mode */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_Config(); USART1_Config(); if (SysTick_Config(SystemCoreClock / 1000)) while (1);while (1)
{ /* Set PC0 and PC1 */ GPIO_WriteBit(GPIOC , GPIO_Pin_13 , (ledVal) ? Bit_SET : Bit_RESET); ledVal = 1 - ledVal; SendChar('f'); Delay(250); }}/* Delay fuction */void Delay(__IO uint32_t nTime){TimingDelay = nTime;while(TimingDelay != 0);}/* Decrement */void TimingDelay_Decrement(void){if (TimingDelay != 0x00)TimingDelay --;}#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) *//* Infinite loop */
while (1) { }}#endif/**
* @} *//**
* @} *//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
void GPIO_Config(void) {
// PC4 configuration (TX)RCC->AHBENR |= 1 << 19; // enable GPIOC clockGPIOC->MODER |= 2 << (4*2); // GPIO_Mode_AFGPIOC->OTYPER |= 1 << (4*1); // GPIO_OType_ODGPIOC->OSPEEDR |= 3 << (4*2); // GPIO_Speed_50MHzGPIOC->PUPDR &= ~(3 << (4*2)); // GPIO_PuPd_NOPULLGPIOC->AFR[0] |= 7 << (4*4); // AF7// PC5 configuration (RX)GPIOC->MODER |= 2 << (5*2); // GPIO_Mode_AFGPIOC->AFR[0] |= 7 << (5*4); // AF7}/* Configuring USART1 */void USART1_Config(void){RCC->APB2ENR |= RCC_APB2ENR_USART1EN; // Enable USART1 clockUSART1->BRR = 72000000/115200;USART1->CR1 &= ~USART_CR1_OVER8; // Oversampling mode = 16USART1->CR1 &= ~USART_CR1_M; // Word length = 8 bitsUSART1->CR2 &= ~(USART_CR2_STOP_1 | USART_CR2_STOP_0); // one stop bitUSART1->CR1 &= ~USART_CR1_PCE; // No parityUSART1->CR1 |= USART_CR1_UE; // USART enableUSART1->CR1 |= USART_CR1_RE; // Receiver enableUSART1->CR1 |= USART_CR1_TE; // Transmitter enable}
uint8_t SendChar (uint8_t ch){ while (!(USART1->ISR & USART_ISR_TXE)); USART1->TDR = (ch & 0xFF); return (ch);}uint8_t GetChar (void){ while (!(USART1->ISR & USART_ISR_RXNE)); return ((uint8_t)(USART1->RDR & 0xFF));}2018-05-14 12:06 AM
that seems there're no any error with my code.
If you mean 'no build error', this is just one step toward a proper working code ...
Have you checked the TX pin of your USART with a scope ?
BTW:
This looks readable, and comprehensible.
void USART1_Config(void){
RCC->APB2ENR |= RCC_APB2ENR_USART1EN; // Enable USART1 clockUSART1->BRR = 72000000/115200;USART1->CR1 &= ~USART_CR1_OVER8; // Oversampling mode = 16USART1->CR1 &= ~USART_CR1_M; // Word length = 8 bits...
But this, a bit 'unconventional':
void GPIO_Config(void) {
// PC4 configuration (TX)RCC->AHBENR |= 1 << 19; // enable GPIOC clockGPIOC->MODER |= 2 << (4*2
); // GPIO_Mode_AFGPIOC->OTYPER |= 1 << (4*1
); // GPIO_OType_ODGPIOC->OSPEEDR |= 3 << (4*2
); // GPIO_Speed_50MHzGPIOC->PUPDR &= ~(3 << (4*2
)); // GPIO_PuPd_NOPULLGPIOC->AFR[0] |= 7 << (4*4
); // AF7...
You are sure you know what you are doing ?
Do you always correct the corresponding comment when you change the Magic Bit Shift Numbers ?
But when I use PL2303 to convert serial-usb for connecting with PC.
The Windows driver for PL2303-based USB-Serial converters seem faulty, it used to crash on my systems after less than a minute. Sometimes with a blue screen.
The Linux driver works fine, though.
2018-05-14 3:19 AM
Hi Avatar, I have found out that I didnt configure PC4 (TxD) in Output Push Pull ( I configured it in Open Drain mode). so I get that problem. Anyway, thanks for your comment. It's very helpful
2018-05-14 3:36 AM
Ahhh yes, forgot to mention that.
OD is useful for I2C or directly driving BJTs/FETs, but not digital periphery.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.