2014-05-08 12:34 AM
Hi, i have a STM32F3Discovery board and i am trying to communicate to a sim900 module. First i am trying to send data serially from the discovery to the computer using hyperterminal on windows 8. I am sending the char ch = 0x49 but on hyper terminal i am receiving the character ''[''.
upon opening my serial window uart1 i can not see anything in it while it is in debug mode and the code is running..is there something i have to specify within hardware or software maybe? // STM32 USART1 (Tx PA.9, Rx PA.10) STM32F3 Discovery - sourcer32@gmail.com #include ''stm32f3_discovery.h'' //**************************************************************************** void Delay(__IO uint32_t nCount); void RCC_Configuration(void) { /* USART1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* GPIOA clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); } //**************************************************************************** void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; /* GPIO Configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect USART pins to AF */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7); // USART1_TX GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7); // USART1_RX } //**************************************************************************** void USART1_Configuration(void) { USART_InitTypeDef USART_InitStructure; /* USARTx configuration ------------------------------------------------------*/ /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); } //**************************************************************************** int main(void) { uint16_t ch; RCC_Configuration(); GPIO_Configuration(); USART1_Configuration(); ch = 0x49; // 'I' while(1) { if (USART_GetFlagStatus(USART1, USART_FLAG_TXE) != RESET) // Check for Empty { Delay(1000); USART_SendData(USART1, ch); // Send Character } } while(1); // Don't want to exit } void Delay(__IO uint32_t nCount) //in millisecond { nCount = nCount * 5940 *2;//381; while(nCount--) { } } //**************************************************************************** #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { } } #endifWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.