2009-12-28 9:03 AM
USART Clock
2011-05-17 4:35 AM
Hi
I have a problem with synchronous USART(on USART3).I have configured related parts, but I have not any output clock whenever I send information via it.(Data can be seen with oscilloscope but clock is not available). I am using Ride7(7.20.09.0162) as a compiler. The part of the program which is related to USART configuration is as follow, and I will appreciate if anybody can help me to find my failure. #define sysclock High void USART_Configuration(void) { USART_InitTypeDef USART_InitStructure; USART_ClockInitTypeDef USART_ClockInitStructure; //USART3 configuration #if(sysclock==High)//36MHz USART_SetPrescaler(USART3, 0x04);//USART Clock set to 4.5MHz ((APB1CLK=18Mhz)/4) #elif(sysclock==Low)//4MHz USART_SetPrescaler(USART3, 0x01);//USART Clock set to 4MHz ((APB1CLK=4Mhz)/1) #endif USART_ClockInitStructure.USART_Clock = USART_Clock_Enable; USART_ClockInitStructure.USART_CPOL = USART_CPOL_High; USART_ClockInitStructure.USART_CPHA = USART_CPHA_2Edge; USART_ClockInitStructure.USART_LastBit = USART_LastBit_Enable; USART_ClockInit(USART3,&USART_ClockInitStructure); USART_InitStructure.USART_BaudRate = Global_Def_USART3_Default_Baud; USART_InitStructure.USART_WordLength = USART_WordLength_9b;//Word Length = 9 Bits USART_InitStructure.USART_StopBits = USART_StopBits_1_5;//1.5 stop bit is transmitted at the end of frame USART_InitStructure.USART_Parity = USART_Parity_Even;//Even parity,When parity is enabled, the computed parity is inserted at the MSB position of the transmitted data (9th bit when the word length is set to 9 data bits; 8th bit when the word length is set to 8 data bits). USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;//Tx and Rx enabled USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;//Hardware flow control disabled (RTS and CTS signals) USART_Init(USART3, &USART_InitStructure); USART_Cmd(USART3, ENABLE);//Enable USART3 } void RCC_Configuration(void) { RCC_DeInit();//RCC system reset(for debug purpose) RCC_HSEConfig(RCC_HSE_ON);//Enable HSE HSEStartUpStatus = RCC_WaitForHSEStartUp();//Wait till HSE is ready if(HSEStartUpStatus == SUCCESS) { RCC_PCLK2Config(RCC_HCLK_Div1);//APB2CLK = HCLK FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);//Enable Prefetch Buffer #if(sysclock==High) RCC_HCLKConfig(RCC_SYSCLK_Div1);//AHBCLK = SYSCLK-36Mhz RCC_PCLK1Config(RCC_HCLK_Div2);//APB1CLK = AHBCLK/2-18Mhz FLASH_SetLatency(FLASH_Latency_2);//Flash 2 wait state RCC_PLLConfig(RCC_PLLSource_HSE_Div2,RCC_PLLMul_9);//PLLCLK = 8MHz/2 * 9 = 36 MHz RCC_PLLCmd(ENABLE);//Enable PLL while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)//Wait till PLL is ready { } RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);//Select PLL as system clock source while(RCC_GetSYSCLKSource() != 0x08)// Wait till PLL is used as system clock source { } #elif(sysclock==Low) RCC_HCLKConfig(RCC_SYSCLK_Div2);//AHBCLK = SYSCLK/2-8Mhz/2=4Mhz RCC_PCLK1Config(RCC_HCLK_Div1);//APB1CLK =AHBCLK-4Mhz FLASH_SetLatency(FLASH_Latency_0);//Flash 0 wait state RCC_SYSCLKConfig(RCC_SYSCLKSource_HSE); #endif } RCC_GetClocksFreq(&RCC_ClocksStatus); HCLK_Freq=(RCC_ClocksStatus.HCLK_Frequency/800000); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE);//TIM2 clock enable RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE);//Enable GPIOA, GPIOB , GPIOD , GPIIOE and AFIO clocks RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO,ENABLE);//Enable GPIOD and AFIO clocks RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3,ENABLE);//Enable USART3 clocks } void GPIO_Configuration(void) { //USART3_Tx GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); //USART3_Rx GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOB, &GPIO_InitStructure); //USART3_Clk GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); }2011-05-17 4:35 AM
Don't you enable as well some other peripheral, that shares the same pins, like SPI, I2C2 etc.? Setting their clock ON means enabling them...
See errata sheet and use pin remapping if needed.2011-05-17 4:35 AM
Thanks for your answer, No, I didnt enable any other shared part with USART3(I2C2 is shared with USART3,and it is disabled(also I checked its clock as well)
2011-05-17 4:35 AM
Which MCU do you use? Is it the same as in your other post? Please post complete sales type.
If it's a ''low density'' STM32 (32kB of FLASH and lower), neither I2C2 nor USART3 are available, supported nor tested. You need at least ''medium density'' (64-128 kB FLASH) device for such operation.2011-05-17 4:35 AM
Thanks, I am using STM32F101VBT6 which is a medium dencity device and has I2C2 as well as USART3.
2011-05-17 4:35 AM
USART1 or 2 in synchronous mode works well? Try as well remapping of USART3 to test whether the CK pin is influenced by something or not. Be aware that after remapping, you need to configure different set of pins.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.