2014-11-22 9:35 AM
Hi
Are some PINs on an unprogrammed device high or low? I have an unprogrammed STM32F4 and a short circuit on the power supply 3.3V, therfore I can't program the chip... Regards2014-11-22 9:50 AM
Short-circuits would tend to be caused by solder, incorrect orientation of the part, and circuit design/fabrication failures.
More than one board?An unprogrammed part is going to have the majority of it's signal lines in input mode, it will crash almost immediately as there is no valid code to execute. The run something you'd need to strap BOOT0 so it enters the System Loader.2014-12-21 11:59 AM
Its ok, a component was soldered wrong. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.