cancel
Showing results for 
Search instead for 
Did you mean: 

Unlocking flash memory (PELOCK bit) on STM32L051T6

Damiano Balzani
Associate III
Posted on March 28, 2018 at 10:35

Hi eveerybody,

I'm tryng to use the protections against unwanted write/erase operations reported on 3.4.3 of Reference manual.

When my program runs the memory is locked (PELOCK BIT = 1) and i want to unlock it.

There is an examole code on reference manual. I copied it on my code but it doesn't work.

This is my code:

while ((FLASH->SR & FLASH_SR_BSY) != 0) /* (1) */

{

   add here time-out management */

}

if ((FLASH->PECR & FLASH_PECR_PELOCK) == 0) /* (2) */

{

     if ((FLASH->PECR & FLASH_PECR_PRGLOCK) != 0) /* (3) */

    {

         FLASH->PRGKEYR = 0x8C9DAEBF; 

         FLASH->PRGKEYR = 0x13141516;

         FLASH->PECR &= !FLASH_PECR_PELOCK;

     }

}

Do i miss something? clocks or enable maybe??

Generally how can i access to FLASH -> PECR register?

Thanks in advance

Damiano

#pelock
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.