2016-09-11 4:50 AM
Hello
I have written a code like this:#include <
stdio.h
>
#include <
string.h
>
#include ''stm32f10x_gpio.h''
#include ''stm32f10x_rcc.h''
#include ''stm32f10x_usart.h''
#include ''stm32f10x_dma.h''
union receive{
unsigned long int Pack;
};
union receive var1;
void check(char data1,char data2){
unsigned long int buffer[17];
buffer[0]=123456;
var1.Pack=buffer[0];
printf(''innn%ld'',var1.Pack);
}
but it returns 1 instead of 123456 or when I fill it with 654321 value it returns again 1.
what is my mistake?
2016-09-11 1:49 PM
This lacks sufficient context to know why exactly it is failing.
I'd suspect it is an issue with the the C startup code initializing things, or the code generation. I would suggest you look at the generated code, and step through the assembler instructions in the debugger to get a better grasp about why it isn't working correctly.2016-09-11 11:12 PM
From the provided example, I fail to grasp the reasoning for using a union.
You could have used a struct, or even a simple integer as well ...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.