2024-05-17 10:37 AM
Hi, I was trying to have microSD logging with F439 Nucleo. I can't see example with mentioned board. Please let me know:
1. example for mentioned board to log data in microSD
2. I tried configuring SD-4 bit, but couldn't identify the pins intialized in generated code (in MX pins used were visible)
3. Tried importing F413 Nucleo e.g., but couldn't identify pins configured and wasn't able to change MCU to F439.
Please guide.
Solved! Go to Solution.
2024-06-05 2:48 AM
Closing post...not getting any replies
2024-05-17 11:01 AM
NUCLEO-F439ZI
https://www.st.com/en/evaluation-tools/nucleo-f439zi.html
https://www.st.com/resource/en/datasheet/stm32f439zi.pdf
Options for SDIO/SDMMC pins going to be very limited
PD2 CMD
PC8 D0
PC9 D1
PC10 D2
PC11 D3
PC12 CLK
GPIO for Socket Card Detect
Usually found at upper end of connectors
2024-05-20 12:23 AM
I mean pin configurations in code, I can see pin assignment in MX and board.
2024-05-20 1:42 AM - edited 2024-05-20 1:47 AM
Callbacks in the MSP code?
For examples look in Applications directory of STM32f4x9 EVAL boards and similar. Going to use materially same pins as few choices.
Check adapter board has pull-ups on data and cmd lines. See schematic for EVAL boards.
2024-05-20 5:25 AM
Thanks (Im new to ST environment and also using new interfaces),
I was able to identify pins in "stm32f4xx_hal_msp.c", will work on:
Understanding uSD SDIO interface configurations in code and
Having R/W e.g. for Nucleo F439.
2024-05-20 10:10 AM
Hello,
You can use CubeMx code generator tool for any board you want by following this video on Youtube especially at the minute 06:00.
2024-05-22 1:23 AM - edited 2024-05-22 1:24 AM
Please check reply to topic
2024-05-22 1:24 AM - edited 2024-05-22 1:28 AM
Hello, I made e.g. with default init on MX for F439 Nucleo, SDIO-4 bit with FATFS as SD card.
Then added init of FATFS_LinkDriver() code with writing to file from FatFs_uSD e.g. of F469 Discovery.
I don't see any pins changing (especially clk). Code flow goes through
FATFS_LinkDriver() > f_mount() > f_mkfs() > if (stat & STA_NOINIT) return FR_NOT_READY;
Please check what am I missing. I have connected microSD through a holder kit, can add pull ups on data and cmd, but should see some pins changing right.
2024-05-22 1:31 AM - edited 2024-05-22 1:36 AM
Please check what am I missing.
Sorry but how could community members check what you are missing if you didn't share your project and your schematics?
2024-05-22 4:11 AM - edited 2024-05-23 2:02 AM
Hi, Thanks for your response, I have attached project. Im now failing at:
if( hsd->SdCard.CardVersion == CARD_V2_X)
{
/* SEND CMD55 APP_CMD with RCA as 0 */
errorstate = SDMMC_CmdAppCommand(hsd->Instance, 0);
if(errorstate != HAL_SD_ERROR_NONE)
{
return HAL_SD_ERROR_UNSUPPORTED_FEATURE; /* error here in SD_PowerON() in "stm32f4xx_hal_sd.c" */
}
}
Also the clock looks 400 kHz, In code settings look to be for 48 MHz. Im directly connecting Nucleo board lines to SD card holder board.
| On SD board | Controller pins | Nucleo board | |
| 3v3 | 3.3 | CN8.7 | CN8.7 |
| gnd | GND | CN8.11 | CN8.11 |
| d0 | D0 | PC8 | CN8.2 |
| d1 | D1 | PC9 | CN8.4 |
| d2 | D2 | PC10 | CN8.6 |
| d3 | D3 | PC11 | CN8.8 |
| d5 | CLK | PC12 | CN8.10 |
| d7 | CMD | PD2 | CN8.12 |
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.