2010-09-12 2:39 PM
understanding the connectivity clock tree
2011-05-17 5:06 AM
What is the diffrence between the signal PLLCLK and PLLVCO ?
One is DOUBLE the other. My copy of RM0008 (Rev 11) clearly indicates that PLLVCO = 2 X PLLCLK, and that PLL3VCO = 2 * PLL3CLK The VCO (Voltage Controlled Oscillator) which the PLL is pumping up/down in frequency to achieve the desired rate using the HSI/HSE as a baseline reference. The VCO works at twice the PLL output to ensure that the mark/space ratio of the output clock is 50:50 The PLL design is almost certainly capable of frequencies significantly higher than the logic portion of the STM32. I have ten year old CMOS SoC designs with PLL's in the 300 MHz region.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.