2017-03-26 9:56 AM
I am looking to determine the accuracy of a sensor using the ADC on an STM32L0. For reference, the datasheet's specified accuracy is here:
https://i.imgur.com/Q1w9Eq5.png
.The sensor outputs a voltage in relation to what it senses. Assuming the sensor's output voltage is error free, I'm trying to understand the error in measurement generated by the ADC. Does the figure 'effective number of bits' mean that I can read the 10 most significant bits of the 12 bit result and assume that number is accurate, i.e. the actual value is within 0.5LSB of the 10 measured bits? How does the hardware calibration routine affect this figure?
Let's say that a 12 bit reading of 348 means a measured value of 4896, a reading of 349 means a measured value of 4880, and a reading of 352 means a value of 4834. Assuming this reading was accurate to ±0.5LSB, this means the measured value is accurate to ±8, correct? If we take the max unadjusted error from the datasheet of ±4LSB (or is it ±2LSB?), this means the measured value is accurate to ±64? If I just round the 12 bit reading to 10 bits and assume it's now accurate to ±0.5LSB, I believe this would result in an error of ±32. Can I do the rounding and then put on the result 'Figure accurate to ±32' and be correct all the time, no matter the error in that particular chip? How does this improve if I calibrate the chip using the hardware routine? I would like to be able to claim as much accuracy as possible without having to manually characterize each chip.
2017-03-27 2:19 AM
While not all datasheets state this explicitly (*) I believe the values given for ADC accuracy are meant after performing the internal calibration.
Also, those values are given for optimal (stable) VDDA/VSSA/VREF+/VREF- and low-impedance and stable VIN and stable temperature. These are externalities given by particular application which may/will introduce additional errors.
You may want to read AN2834.
JW
(*)for example:
STM32F031x DocID025743 Rev 4 - there is a footnote to ADC accuracy table
STM32F405xx/407xx DocID022152 Rev 8 - no such footnote nor any other similar statement
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.