2012-08-17 9:13 AM
Hi there.
I am trying to get the STM32F4 DSP library to work together with the CoIDE (
).Currently I have compiled the DSP math library with GCC using Keil, where I opened the GCC library project.
I've then added the compiled library file, libarm_cortexM4lf_math.a, to the CoIDE project together with the FFT example source code.
I've set the proper definitions: ARM_MATH_CM4, ARM_MATH_MATRIX_CHECK, ARM_MATH_ROUNDING, __FPU_USED
and also selected the ''FPU hard'' compiler command.
Though when I try to compile the project the GCC linker gives me the following error:
[cc] arm-none-eabi-gcc -O0 -nostartfiles -Wl,-Map=STM32F4_FFT.map -mcpu=cortex-m4 -mthumb -LC:\CooCox\CoIDE\workspace\STM32F4_FFT -Wl,--gc-sections -Wl,-TC:\CooCox\CoIDE\workspace\STM32F4_FFT\arm-gcc-link.ld -g -o STM32F4_FFT.elf ..\obj\arm_fft_bin_example_f32.o ..\obj\startup_stm32f4xx.o ..\obj\stm32f4xx_rcc.o ..\obj\stm32f4xx_gpio.o ..\obj\system_stm32f4xx.o ..\obj\syscalls.o ..\obj\arm_fft_bin_data.o ..\obj\misc.o -L..\.. -larm_cortexM4lf_math
[cc] C:\CooCox\CoIDE\workspace\STM32F4_FFT\libarm_cortexM4lf_math.a(arm_cmplx_mag_f32.o): In function `arm_sqrt_f32':
[cc] C:\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Libraries\CMSIS\DSP_Lib\Source\GCC/../../../Include/arm_math.h:5705: undefined reference to `sqrtf'
What can I do about the undefined reference to 'sqrtf'? If I try to use the sqrtf function in my main.c file it doesn't give me any errors as long as I remember ''&sharpinclude ''math.h''.
Has it something to do with the compiling of the library in Keil and then imported into CoIDE (but I used same toolchain)? Maybe something with the folder structure?
The complete project can be found in the following zip file:
http://www.tkjelectronics.dk/uploads/STM32F4_FFT_CoIDE.zip
Thank you in advance.
Best Regards
Thomas Jespersen
#stm32f4-dsp2012-08-17 4:31 PM
Isn't sqrtf() in arm-none-eabi\lib\thumb\v7m\libm.a ?
I'm having deja-vu here, I know I've built a version of the DSP library directly with GNU/GCC and uploaded it here. I'll have to see if I can find it. If you suspect Keil is the problem, build the library in CooCox or directly with GNU/GCC2012-08-18 12:12 AM
If I'm not totally wrong, sqrt (and sqrtf) reside in libm.a, but I can nowhere detect a '-lm' among the compiler/linker flags.
Perhaps you need to add it manually to the project settings.2012-08-20 9:53 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Building CMSIS DSP_LIB for GCC&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=176]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FBuilding%20CMSIS%20DSP_LIB%20for%20GCC&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=176
arm_math.h has arm_sqrt_f32() which uses your current libraries' sqrtf()2012-08-24 12:24 AM
Now I finally succeeded compiling the project with the FPU-hard selected.
I had to manually copy the libm.a, libg.a and libc.a from the GCC\lib\armv7e-m\fpu folder to the project folder to avoid any VFP problems.But now when I run the project I goes to the Default Handler when running this line: arm_cfft_radix4_f32(&S, testInput_f32_10khz); The project, as it is now can be downloaded here:http://www.tkjelectronics.dk/uploads/STM32F4_FFT_CoIDE_V2.zip
Thanks.2012-08-24 1:52 AM
I had to manually copy the libm.a, libg.a and libc.a from the GCC\lib\armv7e-m\fpu folder to the project folder to avoid any VFP problems.
That's not the best way. You could have added ''GCC\lib\armv7e-m\fpu'' to the the library search path, and just add ''-lm'' to your build options.But now when I run the project I goes to the Default Handler when running this line: arm_cfft_radix4_f32(&S, testInput_f32_10khz);
I suggest to step into this function, to get closer to the offending expression/instructions.
Perhaps the FPU is not enabled, or just a plain stack overflow.
2012-08-25 3:06 PM
I have tried stepping into the function, which contains these lines of code.
And you were right, it appeared that it stopped because of the FPU not being enabled in the System initialization (startup code).Now when it is enabled the example works and calculates the FFT max index as it should = 213.But now my question is how this FFT calculation works with my own samples, as it seems to return an odd maximum number - which did work when calculated on the STM32F103 with the DSP library on that.I am calculating the samples array using the sinf() function with a set sampling frequency and wanted wave frequency.Then from the maximum index calculated from the FFT I should be able to calculate the specific frequency which is the maximum by using the known sampling frequency.Though when I do this there is always one single item in the calculated FFT output that is higher than the frequency I have put in, like a harmonic frequency - but why is this FFT output value then higher than the one on the index for the input frequency?Because the number in the FFT output array that is just lower than the highest one is correctly placed inside the index that matches the input frequency.Thanks for your help.2012-08-26 3:34 AM
Your question concerning FFT is not so easy to understand for me, but as I get it, your frequency maximum is not where you expect it.
Have you tried a reference transformation with an external math tool ? I had used Extrema for that, both viewing the sample vector, and the spectre. And I compared the spectres from the stm32f4 app. with that calculated by Extrema. Are you sure to expect the maxima at the correct place, considering the FFT size and sampling frequency ? As I understood it, the arm_cfft_radix4_f32() function 'skips' the negative half of the spectre, just returning [0 ... fs/2].We’re moving the ST Community to a new platform to give you a better and more reliable community experience.