2019-08-09 8:26 AM
how to slove this undefined reference error:
uint16_t SuggestedMaxTxOctets = 0xFB;
uint16_t SuggestedMaxTxTime = 0X148;
hci_le_read_suggested_default_data_length(&SuggestedMaxTxOctets, &SuggestedMaxTxTime);
i am using bluenrg-2
2019-08-09 8:36 AM
Figure out which source or library file the function is supposed to be in, and then ADD that file to the project.
Use find-in-files, check if code is selectively compiled in with a define.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.