2015-10-05 4:54 PM
What's the best state to put GPIOs which aren't connected to a pin on a particular package in? Does it make any sort of difference? I'm concerned primarily with power consumption.
Thanks in advance!2015-10-06 1:47 AM
Hi glaser.austin,
By default, STM32F4 pins are configured as inputs, except some JTAG pins which can impact the power consumption of the device in different power modes because pins are very sensitive to external noise in input mode I/O. To avoid extra I/O current, all pins should be configured as analog input (AIN); in this mode the Schmitt trigger input is disabled, providing zero consumption for each I/O pin.I'd highly recommend you to have a look to thishttp://www.st.com/web/en/resource/technical/document/application_note/DM00096220.pdf
that gives a measuring application that can be customized to measure the current consumption of different STM32F4 power modes, and shows how to best configure the system for each mode.-Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.