2022-07-20 10:38 PM
I am using stm32h745zi-q board and I am working on the full duplex SPI. Here I aa using spi1 and spi4 . I used interrupt based at the spi1 means master side and I used DMA for SPI4 means slave side .
Here I am able to get the complete data in the SPI1 rx buffer but I am missing first 8characters in the SPI4 rx buffer where I used DMA.
Is there anything need to add to get the complete data in the spi4 rx buffer?
Thanks & Regards
SM.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.