2018-04-13 4:36 AM
Hello Guys,
I am facing a little problem here in reading the who_am_I register of the LIS3DSH which is on the development board. Here are the details.
The board I'm using is STM32F40G (ver MB997D). I am using CubeMX to generate the code.
Wiring. SCL -- PA5
SDA -- PA7Master
MasterHeader 3
I2C1_SDA (PINB7) ---------- PA7 (SDA of the sensor)
I2C1_SCL (PINB6) ---------- PA5 (SCL)
3V Pin ---------- PA6 (SEL/SDO)
LIS3DSH
LIS3DSH
2018-04-13 9:03 AM
Cross posted on MEMS with more details
https://community.st.com/0D50X00009XkWS2SAN
2018-04-13 10:01 AM
Sorry for the incomplete post. Can this be deleted by the mods?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.