2018-04-23 12:33 AM
Hi everyone,
I am using STM32L475 B-L475E-IOT01 kit. My problem is that it does not give me sensors values at once. I want to get the temperature, humidity, pressure, accelerometer and gyro at once. But it only gives me 4 sensor values at once. For example, I have to comment out my one of the sensor code then it gives me the sensor values otherwise when I load my code into the kit with 5 sensors code then the user LED is not blinking. There is no error in the code. I run the code for every sensor individually to get the values and it gives me the values. Please help me with this problem.
thank you
2018-04-23 1:02 PM
I don't use that kit, but I guess the code which comes with it is whipped together from portions of Cube with a pinch of FreeRTOS; and that it simply overflew the m�gic pot. Hardly is there an instant solution.
when I load my code into the kit with 5 sensors code then the user LED is not blinking
Maybe start with finding out, exactly why the LED is not blinking.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.