2021-09-09 12:42 PM
From my functioning STM32 (H7) project, I open the .IOC file which spawns STM32CubeMX, which generates a dialog asking:
"This project was setup using STM32Cube firmware FW_H7 V1.9.0. The new STM32Cube V6.3.0 works best with STM32Cube firmware version FW_H7 V1.9.0."
A little confusing considering I am already at V1.9.0, but if I select <Migrate>, then exit CubeMX with <Generate Code>. After rebulilding the project, output of floating point variables no longer work (i.e. displayed as 0.00).
If I select <Continue> (instead of Migrate>, CubeMX just displays a blank screen.
The STM32CubeIDE is v1.7.0.
Note, that I have the -u_printf_float linker option selected/enabled.
This happened a few months ago, and the only solution I found to resolve this issue was to create a new project, and import/copy over all the modules into the new project.
Thanks in advance for you help.
2021-09-10 3:21 AM
>after migrating to latest STM32 FW version.
Don't upgrade FW unless you need to.
>After rebulilding the project,
It's your project. You have to diff and revert or fix the changes you don't agree with.
>output of floating point variables no longer work (i.e. displayed as 0.00).
https://community.st.com/s/question/0D50X0000Anrcyj/how-to-use-float-in-printf
https://community.st.com/s/question/0D50X0000AldaPzSQI/cubeide-sprintf-does-not-work-with-f
2021-09-10 3:34 AM
Is a recurrent problem. Check meta data nodes in project files. Especially ones related to libraries choices, defines, use of nano libs, etc.
Look at .MAP files to get a grasp on what's being pulled in for workings vs non-working builds.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.