2022-12-20 10:46 AM
Hi
I would like to design an ultra low power pulse counter based. The LPTIM is the best option. However, my application require's 4 channels. Is there anyway to achive this with the STM32?
BR
Gilberto
2022-12-20 11:15 AM
Define "ultra low power".
Define requirements on "pulse counter".
JW
2022-12-20 12:23 PM
Hi
The application is gas metering. The pulse frequency is < 1Khz per channel;
The average consumption when counting pulses @ 1Khz on all 4 channels is < 1uA;
BR
Gilberto
2023-01-02 7:33 AM
Hi @GErma.1 ,
STM32U5 has several LPTIM instances, each one with up to 2 independent channels.
The LPBAM feature available for STM32U5 helps to save power. In the AN4865 Low-power timer (LPTIM) applicative use cases on STM32 MCUs and MPUs, you may find examples on the how to.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.