2014-09-20 2:50 AM
With my STM32F4 discovery board I cannot get the UART4_IRQHandler to be triggered on incoming serial data. However the USART2_IRQHandler functions as expected and when the data is ready from the UART4 RX data registered and transmitted out it works without a problem, only the interrupt will not work.
Initialisation++++++++++++++++++++void uartLink_init(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_SetBits(GPIOC, GPIO_Pin_9); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4); GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx; /* USART Rx configuration */ USART_Init(UART4, &USART_InitStructure); /* USART Tx configuration */ USART_InitStructure.USART_Mode = USART_Mode_Tx; USART_Init(USART6, &USART_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable USART */ USART_Cmd(UART4, ENABLE); USART_Cmd(USART6, ENABLE); messageStatus = fingerDataWait;}+++++++++++++++++++++++++++++Interrupt+++++++++++++++++++++++++++++void UART4_IRQHandler(void){ uint8_t data = USART_ReceiveData(UART4); USART_SendData(USART6, data);}+++++++++++++++++++++++++Main loop+++++++++++++++++++++++++int main(void){ prvSetupHardware(); uartLink_init(); power_GPS(POWER_ON); gps_init(); while(1) { if (USART_GetFlagStatus(UART4, USART_FLAG_RXNE) != RESET) { uint16_t x = USART_ReceiveData(UART4); while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET); USART_SendData(USART6, x); } }++++++++++++++++++++++++Interestingly with the GPS unit powered and configured as a serial with an interrupt it does not retrun to the main loop when in the debug state. However On the main application which has a freeRTOS implementation it works without problem. This information is possible inconsiquential to the uart4 fault i am having #irq #stm32f429discovery #uart42014-09-20 11:13 AM
USART_ITConfig(UART4, USART_IT_RXNE, ENABLE);
2014-09-20 5:07 PM
Clive1 you are a scholar and a gentleman.
I dont know how I completely overlooked that 100 times from my other example!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.