2023-04-29 3:03 AM
Project Details:
The project consists of two STM32 MCUs connected over UART (without any external pull up resistors). One STM32L4 MCU (LPUART1) acts as an AT master and other STM32L0 MCU (UART 1) acts as an AT slave. AT slave is configured to wake up from STOP mode on RXNEIE.
Observations:
Question: Why MCU1 LPUART GPIO pin state during the initialization impacting the Receiving/Transmitting or wake up capability of MCU2, connected over UART?
What am i missing? Please guide.
2023-04-29 3:19 AM
Debug the slave as usually. Observe the UART errors. Prolonged log.0 at Rx is BREAK, which in STM32 UARTs acts as a framing error - do you handle that error?
JW
2023-04-29 4:02 AM
Thanks for your insights. Unfortunately i don't have debug pins exposed in the custom board for slave.
I think i can rule out the BREAK error by the following observation, please correct me if otherwise.
Both the boards are power cycled at the same time (as they are connected to same battery source),After the power cycle I manually reset the slave first and wait for significant time till it finishes initialization to enter stop mode. And then i manually reset the Master(to eventually call UART_INIT while having the pin pulled up) works completely fine.
To be precise, the pull up state of the LPUART TX pin before and after the call to LPUART initialization does not have any effect. It only has effect during the call to MX_LPUART1_UART_Init().
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.