2020-09-02 3:56 AM
I have a weight cell connected to NUCLEO-F401RE over UART. I send specific frames and cell responds acording to these ones. I am able to send and receive fixed length frames successfully using HAL_UART_Transmit and HAL_UART_Receive.
The problem is that cell frame length responses are variable. These frames have fixed SOF and EOF (frame always starts with 0x44 and ends with 0x0A) so I tried receiving one byte at a time to detect SOF and EOF using HAL_UART_Receive_IT and push every character into a buffer.
Program does not work because I get overrun error and do not know how to fix it. Is this problem caused by HAL functions? If so, where can I find an example of UART RX interrupt without using HAL?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.