2018-04-20 3:29 AM
Hello,
I am trying to cummunicate with device throught UART, but communication is not working reliably. I am trying to read data continuosly by transmitting request in infinite loop, but I receive incomplete or currupted message. Could you give me some some advice what am I doing wrong?
Here is my code:
int DataRecieved = 0;
int main(void)
{ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USART3_UART_Init(); HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_SET); //RS 485 transmit modewhile (1)
{if(HAL_UART_Transmit_IT(&huart3, (uint8_t*)aTxBuffer, 2) != HAL_OK)
{ while(1); } while(DataRecieved != 0); if(HAL_UART_Receive_IT(&huart3, (uint8_t*)aRxBuffer, 4) != HAL_OK) { while(1); } while(DataRecieved == 0);//Do something with received data
}
Here are my callback functions:
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *UartHandle)
{ /* Set transmission flag: transfer complete */ HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_RESET); //RS 485 receive mode DataRecieved = 0;}void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{ /* Set transmission flag: transfer complete */ HAL_GPIO_WritePin(GPIOB,GPIO_PIN_9,GPIO_PIN_SET); //RS 485 transmit mode DataRecieved = 1;}2018-04-20 4:43 AM
Dear Vaclav
According to me, the functions
HAL_UART_Transmit_IT and
HAL_UART_Receive_IT have to be placed outside the main
infinite loop. Please find attached an example of UART communication tested on a STM32F4 discovery board.
Pins 9 and 10 are connected together to create a loopback on UART1.
Bye
JC
/* Includes ------------------------------------------------------------------*/
#include 'stm32f4xx_hal.h'
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
/* USER CODE BEGIN 0 */
uint8_t tx_buffer[]={0,1,2,3,4,5,6,7,8,9};
uint8_t rx_buffer[10];
/* USER CODE END 0 */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* System interrupt init*/
/* Sets the priority grouping field */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Receive_IT(&huart1,rx_buffer,10);
HAL_UART_Transmit_IT(&huart1,tx_buffer,10);
/* USER CODE END 2 */
/* USER CODE BEGIN 3 */
/* Infinite loop */
while (1)
{
}
/* USER CODE END 3 */
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
}
/* USART1 init function */
void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&huart1);
}
/** Pinout Configuration
*/
void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__GPIOA_CLK_ENABLE();
}
/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
__NOP(); // for debuging only
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
__NOP();// for debuging only
}
/* USER CODE END 4 */
2018-04-20 7:00 AM
I am not sure if I understand completly. If I put functions:
HAL_UART_Receive_IT(&huart1,rx_buffer,10) and HAL_UART_Transmit_IT(&huart1,tx_buffer,10) outside main infinite loop, how do I send another request? I need to send and receive continuously. ShalI I put these functions again in receive callback functions or what?
2018-04-22 3:28 AM
Dear Vaclav
In your case, when you need to transmit and receive continuously, the use of DMA seems to be the best way.
DMA has to be configured in circular mode. The following code has been tested on a nucleo L4 board.
PA9
(USART1_TX)
and PA10 (USART1_RX) connected together.In my example, an integer array of size NSIZE is continuously transmitted and received.
To have more complete explanations, I suggest you to look at the ebook proposed by
Carmine Noveillo Mastering STM32.
JC
/* Includes ------------------------------------------------------------------*/
#include
'main.h'
#include
'stm32l4xx_hal.h'/* USER CODE BEGIN Includes */
#include
<stdio.h>#include
<string.h>/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef
huart1;
UART_HandleTypeDef
huart2;
DMA_HandleTypeDef
hdma_usart1_tx;
DMA_HandleTypeDef
hdma_usart1_rx;
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
#define
NSIZE 20uint8_t
tx_buffer[NSIZE]={0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 9, 8, 7, 6, 5, 4, 3, 2, 1, 0};uint8_t
rx_buffer[NSIZE];__IO
ITStatus
DataReceived =RESET
;/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void
SystemClock_Config(void
);static
void
MX_GPIO_Init(void
);static
void
MX_DMA_Init(void
);static
void
MX_USART2_UART_Init(void
);static
void
MX_USART1_UART_Init(void
);int
main(void
){
HAL_Init();
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
char
msg[80];
sprintf
(msg,
'start \r\n');
HAL_UART_Transmit(&huart2, (
uint8_t
*) msg,strlen
(msg), HAL_MAX_DELAY);HAL_UART_Transmit_DMA(&huart1, tx_buffer, NSIZE);
HAL_UART_Receive_DMA (&huart1, rx_buffer, NSIZE);
/* USER CODE END 2 */
/* Infinite loop */
while
(1){
if
(DataReceived ==SET
){
for
(int
i=0; i<NSIZE; i++){
sprintf
(msg,'value %d : %d \r\n'
, i, rx_buffer[i]);HAL_UART_Transmit(&huart2, (
uint8_t
*) msg,strlen
(msg), HAL_MAX_DELAY);}
memset
(rx_buffer, 0, NSIZE);HAL_Delay(5000);
}
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @
retval
None*/
void
SystemClock_Config(void
){
/* ... */
}
/* USART1
init
function */static
void
MX_USART1_UART_Init(void
){
huart1.
Instance
= USART1;huart1.
Init
.BaudRate
= 115200;huart1.
Init
.WordLength
= UART_WORDLENGTH_8B;huart1.
Init
.StopBits
= UART_STOPBITS_1;huart1.
Init
.Parity
= UART_PARITY_NONE;huart1.
Init
.Mode
= UART_MODE_TX_RX;huart1.
Init
.HwFlowCtl
= UART_HWCONTROL_NONE;huart1.
Init
.OverSampling
= UART_OVERSAMPLING_16;huart1.
Init
.OneBitSampling
= UART_ONE_BIT_SAMPLE_DISABLE;huart1.
AdvancedInit
.AdvFeatureInit
= UART_ADVFEATURE_NO_INIT;
if
(HAL_UART_Init(&huart1) !=HAL_OK
){
_Error_Handler(__FILE__, __LINE__);
}
}
/* USART2
init
function */static
void
MX_USART2_UART_Init(void
){
huart2.
Instance
= USART2;huart2.
Init
.BaudRate
= 115200;huart2.
Init
.WordLength
= UART_WORDLENGTH_8B;huart2.
Init
.StopBits
= UART_STOPBITS_1;huart2.
Init
.Parity
= UART_PARITY_NONE;huart2.
Init
.Mode
= UART_MODE_TX_RX;huart2.
Init
.HwFlowCtl
= UART_HWCONTROL_NONE;huart2.
Init
.OverSampling
= UART_OVERSAMPLING_16;huart2.
Init
.OneBitSampling
= UART_ONE_BIT_SAMPLE_DISABLE;huart2.
AdvancedInit
.AdvFeatureInit
= UART_ADVFEATURE_NO_INIT;
if
(HAL_UART_Init(&huart2) !=HAL_OK
){
_Error_Handler(__FILE__, __LINE__);
}
}
/**
* Enable DMA controller clock
*/
static
void
MX_DMA_Init(void
){
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt
init
*//* DMA1_Channel4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(
DMA1_Channel4_IRQn
, 0, 0);HAL_NVIC_EnableIRQ(
DMA1_Channel4_IRQn
);/* DMA1_Channel5_IRQn interrupt configuration */
HAL_NVIC_SetPriority(
DMA1_Channel5_IRQn
, 0, 0);HAL_NVIC_EnableIRQ(
DMA1_Channel5_IRQn
);}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
static
void
MX_GPIO_Init(void
){
GPIO_InitTypeDef
GPIO_InitStruct;/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin,
GPIO_PIN_RESET
);/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.
Pin
= B1_Pin;GPIO_InitStruct.
Mode
= GPIO_MODE_IT_FALLING;GPIO_InitStruct.
Pull
= GPIO_NOPULL;HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.
Pin
= LD2_Pin;GPIO_InitStruct.
Mode
= GPIO_MODE_OUTPUT_PP;GPIO_InitStruct.
Pull
= GPIO_NOPULL;GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_LOW;HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : PC5 */
GPIO_InitStruct.
Pin
= GPIO_PIN_5;GPIO_InitStruct.
Mode
= GPIO_MODE_AF_PP;GPIO_InitStruct.
Pull
= GPIO_NOPULL;GPIO_InitStruct.
Speed
= GPIO_SPEED_FREQ_VERY_HIGH;GPIO_InitStruct.
Alternate
= GPIO_AF7_USART3;HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
void
HAL_UART_RxCpltCallback(UART_HandleTypeDef
*huart){
__NOP();//for debugging only
if
(huart==&huart1){HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin,
GPIO_PIN_SET
);DataReceived =
SET
;}
}
void
HAL_UART_TxCpltCallback(UART_HandleTypeDef
*huart){
__NOP();//for debugging only
if
(huart==&huart1){HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin,
GPIO_PIN_RESET
);DataReceived =
RESET
;}
}
2018-04-24 4:00 AM
Thank you very much Jean-Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.