2022-03-13 6:24 PM
Hello
I want to use two STM32F407 MCUs to enable bidirectional communication via UART communication with each other.
I would like to have a two-way communication that turns on and off each other by installing a switch and an LED, respectively. Thanks a lot for your advice. thank you.
2022-03-13 8:24 PM
Aren't there literally hundreds of UART examples you could use as a starting point?
Have a common ground and cross-connect the RX and TX between the two STM32 parts
2022-03-15 4:21 AM
Hello @�?� 정훈,
I recommend you referring to the UART examples provided by the STM32CubeF4.
For example you can find them under the "STM32CubeF4/Projects/STM32F401-Discovery/Examples/UART" root.
Please follow the instructions mentioned in the readme file.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.