2012-12-09 4:57 PM
The manual says that the STM32 supports only 8 and 9 word length for UART.
But I need 7 data bits.How can I configure the 7 data bits? #7-databits-uart-usart2012-12-09 6:25 PM
Presumably by configuring as 8-bit and have the eighth bit being stuffed as a extra stop bit?
USARTx->DR = x | 0x80; // Add High Stop bit .. x = USARTx->DR & 0x7F;2012-12-09 10:21 PM
Thank you for help.
But there might be framing errors when the counter part UART transmits 1 start, 7 data bits and 1 stop bit.The 1 stop bit might be considered as the 8th data bit by the STM UART side.And it might expect ''1 stop bit''(signal HIGH).If the counter UART start to transmit another byte by sending STX (signal LOW) in this moment, then there might be framing error.How do you think about this scenario?2012-12-10 6:32 AM
How do you think about this scenario?
I think you are going to have to evaluate it, and validate it to your own satisfaction, the STM32's don't have a 7N1 configuration.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.