2013-06-18 11:51 AM
2013-06-18 11:59 AM
The thread is poorly titled.
The uart_puts() routine is broken by a cut-n-paste failure, it's suppose to use a character pointer. You don't actually initialize the USART. And you assume that printf() magically routes to an arbitrary USART. You could sprintf() to a buffer and use uart_puts() to be tool chain agnostic.2013-06-18 12:50 PM
2013-06-18 6:07 PM
Now that you have gotten this far - here is a simple debugging technique. You have an input from a device to be sent to a usart for verification. Use a watch window on the ADCConvertedValues buffer in debug mode to verify that the accelerometer inputs have been properly received before being sent to the usart.
The Discovery kit has a gotcha - some of the pins are dedicated to board functions. PCO/ADC123_IN10 pin is pulled up to 3V for the user USB function. The pins for ADC channels 1, 2, 3, 11, 12, 14 & 15 plus the 8 & 9 you are currently using are freely available. There is a table in the F4 Discovery User Manual that identifies board pin functions. Cheers, Hal2013-06-19 6:16 AM
This should be workable. Please pay attention to ADC channels/pins usable (PB2 is not).
// STM32F4-Discovery ADC3 - sourcer32@gmail.com
#include ''stm32f4xx.h''
#include <
stdio.h
> // sprintf
//******************************************************************************
void USART2_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* enable peripheral clock for USART2 */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* GPIOA Configuration: USART2 TX on PA2 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART2 pin to AF2 */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); // PA2 (USART2_TX)
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2, ENABLE); // enable USART2
}
//******************************************************************************
void USART2_SendString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2, *s++);
}
}
//******************************************************************************
volatile uint16_t ADCConvertedValues[3];
//******************************************************************************
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC, ENABLE);
/* Configure ADC1 Channel8 pin as analog input PB0 *****************************/
/* Configure ADC1 Channel9 pin as analog input PB1 *****************************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Configure ADC1 Channel12 pin as analog input PC2 *****************************/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
//******************************************************************************
void ADC1_Configuration(void)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable peripheral clocks *************************************************/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* DMA2_Stream0 channel0 configuration **************************************/
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0];
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 3;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/* ADC Common Init **********************************************************/
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC1 Init ****************************************************************/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE; // Multiple Channels
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; // Keep Sampling
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 3;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel configuration ******************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_8, 1, ADC_SampleTime_480Cycles); // PB0
ADC_RegularChannelConfig(ADC1, ADC_Channel_9, 2, ADC_SampleTime_480Cycles); // PB1
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 3, ADC_SampleTime_480Cycles); // PC2 (BANKC)
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 **************************************************************/
ADC_Cmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
}
//******************************************************************************
int main(void)
{
USART2_Configuration();
GPIO_Configuration();
ADC1_Configuration();
while(1) /* Infinite loop */
{
if (ADCConvertedValues[2] != 0xFFFF) // Check for new values loaded
{
char string[32];
sprintf(string, ''%03X %03X %03
X'', ADCConvertedValues[0], ADCConvertedValues[1], ADCConvertedValues[2]);
USART2_SendString(string);
ADCConvertedValues[2] = 0xFFFF; // Invalidate
}
}
}
/**************************************************************************/
2013-06-19 2:07 PM
2013-06-19 2:16 PM
hello when i dump this program in stm32discovery board ..i get this error please fix it ..and please suggest me which tool chain should i use...and the error is here:-
NMP, I'm using Keil with a project structure and settings which comport with those of the template projects.2013-06-20 3:18 AM
i am using coocox ..in coocox i am getting a error ..which i have shown you in last post .please fix it
2013-06-20 4:47 AM
i am using coocox ..in coocox i am getting a error ..which i have shown you in last post .please fix it
Sorry, but this really isn't my problem, I'm not here to provide support for the clowns at CooCox, and their broken tool. Seek support from CooCox. This isn't even a problem unique to my code, you had the same problem here [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/stm32%20adc%20multi%20channel&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx¤tviews=147#%7b314E8D1E-6C89-4834-8847-88E5E4FCD317%7d]sharma.vaibhav : stm32 adc multi channel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.