2017-08-06 12:35 PM
There seems to be a typo in UM1670 - Discovery kit with STM32F429ZI MCU, Section 6.7. (TFT LCD).
It says 'The STM32F429ZIT6 controls this motion sensor through the SPI interface.' But it talks about ILI9341 LCD controller, witch is NOT a motion sensor. Yes, ILI9341 can be controlled via SPI, but its performance is better when used on LTDC. This line seems to be a copy-paste typo from the section above that talks about gyroscope mems and IS NOT the best representation of ILI9341.
#stm32f429-disco2017-08-08 3:07 AM
Hi
Fedoseev.Alexand
,Thanks for highlighting this typo. It will be fixed in coming UM version.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.