2018-02-12 1:44 AM
Hi,
it seems in theSTM32Cube_FW_L1_V1.8.1 in Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ex.c there is a typo in the parameter guarding.
in line 811:
HAL_StatusTypeDef HAL_FLASHEx_DATAEEPROM_Erase(uint32_t TypeErase, uint32_t Address)
{
HAL_StatusTypeDef status = HAL_OK;
/* Check the parameters */
assert_param(IS_TYPEPROGRAMDATA(TypeErase));
assert_param(IS_FLASH_DATA_ADDRESS(Address));�?�?�?�?�?�?�?
IS_TYPEPROGRAMDATA()
should be: IS_TYPEERASEDATA()
to STM team:
- can you confirm this typo?
Thanks,
Sven
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.