2010-02-11 11:15 AM
Two Projects, Two .mot files, one Micro
2011-05-17 4:40 AM
Couple of thoughts.
The S5 record contains a count of preceding lines, if you join two files either correct it, or remove it. Dump the content of the entire flash space via serial port or JTAG, and validate it. Checksum or CRC the two parts to observed if there is any measurable difference between loading the individual parts, or the monolithic part. Write a parser for your Motorola HEX file that runs on a PC, not difficult, and load it into memory. Verify that it parses correctly, that addresses do no overlap each other. Generate some more automatic linkage to you secondary main() function so you don't have to manually pull if from the linker or map file when ever it changes. Define a jump or pointer at a fixed offset in startup.s, or whatever. .. DCD SVCHandler ; SVCall Handler DCD DebugMonitor ; Debug Monitor Handler DCD 0 ; Reserved DCD PendSVC ; PendSV Handler DCD SysTickHandler ; SysTick Handler IMPORT main DCD main ; +0x40 - Entry Point for C main() function -Clive2011-05-17 4:40 AM
Thanks Clive.
I have implemented checksums in both the boot and the main app. they are fine, and work as projects by themselves.
When combining the .mot files, I dump the S7 record from the boot, keep the one from the main app, so the mot looks like
S0:MAIN
S3:MAIN
S3:MAIN
S3:BOOT
S7:MAIN
The combined .mot doesn't have any overlap, and all gaps are filled with FFs.
Like I said, the two projects are completely seperate, so they both contain interrupt vectors (two different sets) and both contain complete initializations for the micro. Could that be part of the problem? Do I need to un-initalize the one vector table before initializing a new one? same with system ticks?
2011-05-17 4:40 AM
The app note AN2557 has been suggested in other threads.
Things to watch for are the initialization of the stack. The problem with calling main() directly is that ignores the other things the CRT (C Runtime) is doing. Mainly things like copying data from the static segment into RAM, and zeroing outuninitalized
data. Calling __main might make more sense. Are you using interrupts in the boot loader? Are you initializing clocks, PLLs, etc in the boot loader? I've seen problems where people assume they are running from the HSI clock, and program the PLL. This is a big problem if you are currently running from the PLL. You have to bypass it, or switch to another clock first. The following assembler code could be used to start an image with it's own vector table at the front end. You could put it in the startup.s (or whatever it's called), and call it from C, void RunAppCode(void) RunAppCode PROC EXPORT RunAppCode LDR R0, =0x801B800 ; Boot Vector SP/PC LDR SP,[R0, #0] LDR R0,[R0, #4] BX R0 ENDP -Clive2011-05-17 4:40 AM
I'm almost embarassed to admit what the issue was.... __disable_interrupt(); was not being called before the jump...
grumble...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.