2020-05-04 4:05 PM
Hello! I am trying to implement a phase-shifting full bridge on the STM32F334 microcontroller using HRTIM. Two PUSH-PULL outputs and a phase shift between them, this is necessary for the LLC converter.
I configured the master timer as an event source for timers A and B
Configured timer A and B as PUSH-PULL output.
Event source for setting the output of timers A and B MSTCMP1 and MSTCMP2.
By changing the value in MSTCMP2, I change the phase shift between timers A and B.
This works, but periodically when changing the value of MSTCMP2, I get a phase shift between phases of 180 degrees and not the one that set it. For example, instead of reducing power to 10% percent, I get 90%.
Do you know what you are doing or can help.
Code below:
/* DLL calibration: periodic calibration enabled, period set to 14µs */
HRTIM1->HRTIM_COMMON.DLLCR = HRTIM_CALIBRATIONRATE_14 | HRTIM_DLLCR_CALEN;
/* Check DLL end of calibration flag */
while(HRTIM1->HRTIM_COMMON.ISR & HRTIM_ISR_DLLRDY == RESET);
/* ---------------------------------------------------------------- */
/* Master timer initialization: */
/* ---------------------------------------------------------------- */
HRTIM1->HRTIM_MASTER.MPER = MULTIPHASE_PERIOD;
HRTIM1->HRTIM_MASTER.MREP = REPETITON_RATE;
HRTIM1->HRTIM_MASTER.MCR = HRTIM_MCR_CONT;
/* Set compare registers for phase-shifts in master timer */
/* Each compare is coding for the phase-shift of one phase */
///////////////////////////
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].PERxR = PHASE_PERIOD;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].REPxR = 0; // 1 ISR every REPETITON_RATE PWM periods
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].TIMxCR =HRTIM_TIMCR_PSHPLL;// +HRTIM_TIMCR_RETRIG HRTIM_TIMCR_PREEN + HRTIM_TIMCR_MSTU + ;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].RSTxR = HRTIM_RSTR_MSTCMP1;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].SETx1R = HRTIM_SET1R_MSTCMP1;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].RSTx1R = HRTIM_RST1R_CMP1;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].SETx2R = HRTIM_SET2R_MSTCMP1;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].RSTx2R = HRTIM_RST2R_CMP1;
// TIMERB initialization: Idem Timer A
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].PERxR = PHASE_PERIOD;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].TIMxCR = HRTIM_TIMCR_PSHPLL + HRTIM_TIMCR_PREEN + HRTIM_TIMCR_MSTU + HRTIM_TIMCR_CONT; // HRTIM_TIMCR_RETRIG +
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].RSTxR = HRTIM_RSTR_MSTCMP2;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].SETx1R = HRTIM_SET1R_MSTCMP2;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].RSTx1R = HRTIM_RST1R_CMP2;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].SETx2R = HRTIM_SET2R_MSTCMP2;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].RSTx2R = HRTIM_RST2R_CMP2;
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_A].CMP1xR = duty_c; // Set compare registers for duty cycle
HRTIM1->HRTIM_TIMERx[HRTIM_TIMERINDEX_TIMER_B].CMP1xR = duty_c;
HRTIM1->HRTIM_MASTER.MCMP1R = 100;
HRTIM1->HRTIM_MASTER.MCMP2R = 100;
HRTIM1->HRTIM_COMMON.CR2 |= HRTIM_CR2_MRST
+ HRTIM_CR2_TARST
+ HRTIM_CR2_TBRST;
/* ---------------*/
/* HRTIM start-up */
/* ---------------*/
/* Force register update before starting */
HRTIM1->HRTIM_COMMON.CR2 |= HRTIM_CR2_TASWU
+ HRTIM_CR2_TBSWU
+ HRTIM_CR2_TCSWU
+ HRTIM_CR2_TDSWU;
HRTIM1->HRTIM_COMMON.OENR = HRTIM_OENR_TA1OEN | HRTIM_OENR_TA2OEN | HRTIM_OENR_TB1OEN | HRTIM_OENR_TB2OEN;
/* Start HRTIM's TIMER A, B, C, D */
HRTIM1->HRTIM_MASTER.MCR |= HRTIM_MCR_MCEN | HRTIM_MCR_TACEN | HRTIM_MCR_TBCEN;// | HRTIM_MCR_TCCEN | HRTIM_MCR_TDCEN;
2025-02-10 1:47 AM
Similar issue here, did you managed @APota.1 ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.