2017-05-06 7:24 AM
Hello,
i'm using STM32F4Discovery with the OV7670 camera , i'm trying to get a QVGA picture (320*240) RGB (each pixel is coded in one byte) and then i'll try to send thses picture to a server using SIM900, the probleme is that when i set a breakpoint at the DMA2_ IRQhandler the breakpoint is never reached although the register TCIF1 is set , and that mean that trasfert is done.
i attached my code for more detailsis there somone who could help methank you
############################################################################################
void DCMI_Configure(uint32_t *frame)
{ DCMI_InitTypeDef DCMI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; DMA_InitTypeDef DMA_InitStructure; DMA_InitTypeDef DMA_InitStructureusart; NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitTypeDef NVIC_InitStructureDcmiToDma; /* Enable DCMI GPIOs clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOE, ENABLE);/* Enable DCMI clock */
RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_DCMI, ENABLE);/* Connect DCMI pins to AF13 ************************************************/
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_DCMI);//HSYNC GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_DCMI);//PCLK GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_DCMI);//VSYNC //RED GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_DCMI);//D0 GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_DCMI);//D1 GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_DCMI);//D2//Blue
GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_DCMI);//D3 GPIO_PinAFConfig(GPIOE, GPIO_PinSource4, GPIO_AF_DCMI); //D4GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_DCMI); //D5
GPIO_PinAFConfig(GPIOE, GPIO_PinSource5, GPIO_AF_DCMI);//D6 GPIO_PinAFConfig(GPIOE, GPIO_PinSource6, GPIO_AF_DCMI);//D7 /* DCMI GPIO configuration **************************************************//* D0 -- PC6 D1 -- PA10 D2 -- PC8 D3 -- PC9 D4 -- PE4 D5 -- PB6 D6 -- PE5 D7 -- PE6 PCK - PA6 HS -- PA4 VS -- PB7*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_10 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_Init(GPIOB, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_8 | GPIO_Pin_9;
GPIO_Init(GPIOC, &GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_4;
GPIO_Init(GPIOE, &GPIO_InitStructure);/* PCLK(PA6) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOA, &GPIO_InitStructure); /* DCMI configuration *******************************************************/ DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_SnapShot;//DCMI_CaptureMode_Continuous;//DCMI_CaptureMode_SnapShot; DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware; DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Falling; DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High; DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_High; DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_1of4_Frame; //DCMI_CaptureRate_All_Frame; DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_8b; DCMI_Init(&DCMI_InitStructure);/* DCMI Interrupts config ***************************************************/
DCMI_ITConfig(DCMI_IT_VSYNC, ENABLE); DCMI_ITConfig(DCMI_IT_LINE, ENABLE); DCMI_ITConfig(DCMI_IT_FRAME, ENABLE); DCMI_ITConfig(DCMI_IT_ERR, ENABLE); /* Configures the DMA2 to transfer Data from DCMI to Memory ****************/ /* Enable DMA2 clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); /* DMA2 Stream1 Configuration */ DMA_DeInit(DMA2_Stream1);DMA_InitStructure.DMA_Channel = DMA_Channel_1;
DMA_InitStructure.DMA_PeripheralBaseAddr =(uint32_t)(DCMI_BASE + 0x28);//(DCMI_BASE + 0x28);//DCMI->DR; //DCMI_DR_ADDRESS;//(uint32_t)(&DCMI->DR); DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)frame; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 19200;//25344*3;//320*240*2;//0xfffe; //= Image size /4 //0xfffe; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;//DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;// First take one picture//DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream1, &DMA_InitStructure); DMA_ITConfig(DMA2_Stream1,DMA_IT_TC,ENABLE); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); NVIC_InitStructureDcmiToDma.NVIC_IRQChannel = DMA2_Stream1_IRQn; NVIC_InitStructureDcmiToDma.NVIC_IRQChannelPreemptionPriority = 2;//1 NVIC_InitStructureDcmiToDma.NVIC_IRQChannelSubPriority = 2;//1 NVIC_InitStructureDcmiToDma.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); NVIC_InitStructure.NVIC_IRQChannel = DCMI_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}#########################################################################################'
void DMA2_Stream1_IRQHandler(void)
{//Test on DMA2 Channel1 Transfer Complete interrupt
if(DMA_GetITStatus(DMA2_Stream1,DMA_IT_TCIF1) == SET) { // USART_SendData(USART2, DMA2->); DMA_ClearITPendingBit(DMA2_Stream1,DMA_IT_TCIF1); } if(DMA_GetITStatus(DMA2_Stream1,DMA_IT_TEIF1) == SET) { //USART_SendData(USART2, buff[0]);//TM_USB_VCP_Send(&buff[0], 255); DMA_ClearITPendingBit(DMA2_Stream1,DMA_IT_TEIF1); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.