2018-05-10 5:16 AM
Hello everyone,
I am trying to transmit a string with the UART7 with the DMA on a STM32H743-NUCLEO144 demoboard, to do this I have shorted the pins PF6 and PF7 on the Morpho connector CN11 (short circuit between TX and RX of the UART7). I initialized the components and tried to send a string to DMA, but nothing is transmitted.What did I do wrong?I enclose complete project for Atollic 9.0.0.Thank youWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.