2016-06-18 2:41 AM
What would happen, if PLLMUL is set slightly too large? Let say, if maximum frequency of a MCU is 72 MHz, but PLLMUL is set such that the frequency would be 80 MHz?
Thanks2016-06-18 3:50 AM
At some point you will encounter a critical path in the design, it will not catch fire, it will simply malfunction either in a subtle or spectacular fashion.
Think of it as a bus service with a rigid schedual, if you are not at the bus stop on time you will be left behind, and sometimes you can't run fast enough based on the conditions and length of the path you are running on. Think part of the circuit you are using, along with temperature, voltage and transistor characteristics.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.