2008-01-28 6:51 AM
timers and clocks
2011-05-17 3:22 AM
Hi lior.b,
Yes, this is possible. You should modify the multiplier from x2 to x1 before the Timer clock input to have 18MHz. STOne-32.2011-05-17 3:22 AM
hello,
i tried to run the example1 of the TIM in the FWLIB and it is work correct but there is something that i dont understand APB1 (PCLK1) IS DIVIDED by 4 so the TIM 2,3,4 clock is 72M/4 = 18M but I see that the clock of the timers is 36MHZ. please tell me what i miss here to understand this? please see this configuration (for the example1 in TIM libary) /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); /* Flash 2 wait state */ FLASH_SetLatency(FLASH_Latency_2); /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); //APB Low speed prescaler /* PCLK2 = HCLK */ RCC_PCLK2Config(RCC_HCLK_Div1); //PCLK2 NOT DIVIDED /* PCLK1 = HCLK/4 */ RCC_PCLK1Config(RCC_HCLK_Div4);//PCLK1 = HCLK/4 /* PLLCLK = 8MHz * 9 = 72 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); /* Enable PLL */ RCC_PLLCmd(ENABLE);//turn on the PLL2011-05-17 3:22 AM
thanks for your answer.
but how i multiply the TIMER x2. which register do this?2011-05-17 3:22 AM
Quote:
On 23-01-2008 at 18:17, Anonymous wrote: Hi lior.b, Yes, this is possible. You should modify the multiplier from x2 to x1 before the Timer clock input to have 18MHz. STOne-32. Dear lior.b, Sorry for the confusion, I made a mistake ,in fact This is fixed automatically by hardware to x2 when APB prescaler is different from 1 and is equal to one when APB Prescaler is = 1. So to have a 18MHz you should configure your AHB clock to 18MHz anndAPB = 18MHz but this is not efficient. Hope this clarifies more. STOne-322011-05-17 3:22 AM
This finally makes sense to me. I've been scouring the manual for a couple of hours now trying to find something that confirms your statement. Can you tell me which section I should look at closer ?
btw: this is my first experience w/st mcu's and I'm quite impressed so far, just looking forward to an stm w/an external mem interface.2011-05-17 3:22 AM
Here you go : Page 50 of the reference manual.
2011-05-17 3:22 AM
hello ,
thanks again . i find it and i understood it thank you very much.2011-05-17 3:22 AM
In example number 5 for TIMx peripherals in the FW library, there is this comment block:
/* --------------------------------------------------------------- TIM2 Configuration: Output Compare Timing Mode: TIM2CLK = 36 MHz, Prescaler = 4, TIM2 counter clock = 7.2 MHz CC1 update rate = TIM2 counter clock / CCR1_Val = 146.48 Hz CC2 update rate = TIM2 counter clock / CCR2_Val = 219.7 Hz CC3 update rate = TIM2 counter clock / CCR3_Val = 439.4 Hz CC4 update rate = TIM2 counter clock / CCR4_Val = 878.9 Hz --------------------------------------------------------------- */ Where do they get 7.2MHz from if the main clock is 72MHz and prescaler for APB1 clocks is 4, TIM2CLK is indeed 36MHz but 36/4 = 9, not 7.2.2011-05-17 3:22 AM
Nevermind. I see now that the prescaler is actually the specified value plus one, giving 36/5 = 7.2MHz.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.