2012-01-22 12:00 PM
I'd like to see some sample code (or a link to it) that utilizes a timer fed by an external clock, not the system clock, to generate an output pulse. All ST's sample code that I've seen so far uses the system clock. Here's what I'm trying to do:
Input clock = 5.12MHz, 50% duty cycleOutput clock = 1KHz, very low duty cycleOnce set up, the timer needs to free run, that is, not generate interrupts or require further software to maintain.Any help is much appreciated. #stm32vldiscovery #external-clock #stm32-timer #pwm-output #timer #stm32vldiscovery #stm32vldiscovery2012-01-23 10:34 AM
You should be able to use one of the TIMx_CHx pins to pull in an external clock (mode 1), or TIMx_ETR pins to pull in an external clock (mode 2).
That would supply the timebase, then program one of the channels in PWM where you can program the pulse width (nee duty). If you use prescalers/dividers of one you'd get a programmable granularity of ~195 ns.2012-01-23 5:06 PM
Thanks Clive. ~195nS granularity would be sweet!
I have been able to get a 1KHz output, but only in toggle mode, so 50% d/c. PWM modes aren't working for me so far. I'll try to post some setup code in a bit.JonPS At the same time, I'm also using all 3 UARTS in interrupt mode; they work great!2012-01-23 6:58 PM
Here is code that I have working so far (using Atollic TrueStudio). The external clock I'm using here is actually 10.24MHz; it's divided down to 5.12MHz for use elsewhere.
//Enable Clock for Timer4
RCC_APB1PeriphClockCmd (RCC_APB1Periph_TIM4, ENABLE); // TIM4_CH1 pin (PB.06) configuration GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); // TIM4_CH2 pin (PB.07) configuration GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); //Time base configuration TIM_TimeBaseStructure.TIM_Period = 5120; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); // External Trigger set to External Clock, Mode 1 TIM_ETRClockMode1Config (TIM4, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); // Input Trigger selection TIM_TIxExternalClockConfig (TIM4, TIM_TS_TI2FP2, TIM_ICPolarity_Rising, 0) ; // TIM4 PWM2 Mode configuration: Channel1 TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 2000; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM4, &TIM_OCInitStructure); // Output compare preload enable TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable) ; TIM_OC1FastConfig (TIM4, TIM_OCFast_Enable); // One Pulse Mode selection TIM_SelectOnePulseMode(TIM4, TIM_OPMode_Repetitive); // Output Trigger selection TIM_SelectOutputTrigger(TIM4, TIM_TRGOSource_OC1); // Slave Mode selection: Trigger Mode TIM_SelectSlaveMode(TIM4, TIM_SlaveMode_External1); TIM_Cmd (TIM4, ENABLE);Thanks for the help.JonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.