2013-02-26 12:26 PM
Hello!
Use stm32f107vc.
I'm trying to synchronize two
timers
(TIM3 and TIM5), as including the externaltrigger
. Configure them, as described in RM0008page
386:void TIM3(void)
{
RCC->APB1ENR |= RCC_APB1ENR_TIM3EN;
TIM3->PSC = 70 - 1;
TIM3->ARR = 25000 - 1;
TIM3->DIER &=~ TIM_DIER_UIE;
// (MMS=001)
TIM3->CR2 |= TIM_CR2_MMS_0; /*!<Bit 0 */
TIM3->CR2 &=~ TIM_CR2_MMS_1; /*!<Bit 1 */
TIM3->CR2 &=~ TIM_CR2_MMS_2; /*!<Bit 2 */
// (TS=100)
TIM3->SMCR &=~ TIM_SMCR_TS_0; /*!<Bit 0 */
TIM3->SMCR &=~ TIM_SMCR_TS_1; /*!<Bit 1 */
TIM3->SMCR |= TIM_SMCR_TS_2; /*!<Bit 2 */
// (SMS=110)
TIM3->SMCR &=~ TIM_SMCR_SMS_0; /*!<Bit 0 */
TIM3->SMCR |= TIM_SMCR_SMS_1; /*!<Bit 1 */
TIM3->SMCR |= TIM_SMCR_SMS_2; /*!<Bit 2 */
// (MSM=1)
TIM3->SMCR |= TIM_SMCR_MSM;
TIM3->CNT = 0;
}
void TIM5 (void)
{
RCC->APB1ENR |= 1<<3;
TIM5->PSC = 70 - 1;
TIM5->ARR = 25000 - 1;
TIM5->DIER &=~ TIM_DIER_UIE;
// (TS=001)
TIM5->SMCR |= TIM_SMCR_TS_0; /*!<Bit 0 */
TIM5->SMCR &=~ TIM_SMCR_TS_1; /*!<Bit 1 */ // TS=001
TIM5->SMCR &=~ TIM_SMCR_TS_2; /*!<Bit 2 */
// (SMS=110)
TIM5->SMCR &=~ TIM_SMCR_SMS_0; /*!<Bit 0 */
TIM5->SMCR |= TIM_SMCR_SMS_1; /*!<Bit 1 */
TIM5->SMCR |= TIM_SMCR_SMS_2; /*!<Bit 2 */
TIM5->CNT = 0;
}
As a result,
taking
the registers at the request of both CNT timers USART to get these values:if
TIM5-> ARR = 25000 - 1, and TIM3-> ARR = 25000 - 1; register values CNT same (eg,TIM5_CNT=
0x5936 andTIM3_CNT=
0x5936 orTIM5_CNT=
0x728 andTIM3_CNT=
0x728).but
if
TIM5-> ARR = 50000 - 1, and TIM3-> ARR = 25000 - 1; register values CNT, in theory, should differ by 25000 (0x61A8
), but really they are, for example, like this -TIM5_CNT=
0x22D4 andTIM3_CNT=
0x216F or such -TIM5_CNT=
0x556D andTIM3_CNT=
0xB5B0(0x22D4 - 0x216F = 0xDE (222) and 0xB5B0 - 0x556D = 0x6043(24643))
.In what could be the problem? Maybe something is wrong configured?
2013-02-26 1:20 PM
Some basic math issues there
0x216F
-0x22D4
= 0xFE9B (-357) Add 25000 = 246430xB5B0 - 0x556D = 0x6043 (24643)
With the computation backward (first - second)0x22D4 - 0x216F
= 0x0165 (357)2013-02-26 1:48 PM
Thank you find a mistake, but what can you say about the fact that the difference of registers CNT not 25000, but 24643 (or 357)?
2013-02-26 2:38 PM
From the code the delta is more likely due to disparity in the initialization time.
TIM3->CNT = TIM5->CNT = 0; // would be somewhat more synchronous, yet still not entirely atomic2013-02-27 12:01 AM
Timers are initialized by external trigger.
Initialization with TIM5-> ARR = 25000 - 1 and TIM3-> ARR = 25000 - 1 runs perfectly, but at values TIM5-> ARR = 50000 - 1 and TIM3-> ARR = 25000 - 1 appears delay. can this be? and what to do?2013-02-27 8:17 AM
Use Reset mode instead of Trigger mode?
Are you trying to get them to reset together or start together? The TRGO fabrics would be more consistent if both your timers were slaved and used a common signal. That or masters triggered from two pins tied together. The VL doesn't have a TIM5, but built a TIM3/TIM2 chain that behaves the same way you describe.2013-02-28 2:50 AM
Are you trying to get them to reset together or start together?
I'm trying to start them together.The TRGO fabrics would be more consistent if both your timers were slaved and used a common signal. That or masters triggered from two pins tied together.
This idea occurred to me, but thedocumentation clearly describes a synchronous connection of timers, andit should work, but it does not work.The VL doesn't have a TIM5, but built a TIM3/TIM2 chain that behaves the same way you describe.
Not VL, but VC
.The VL doesn't have a TIM5, but built a TIM3/TIM2 chain that behaves the same way you describe.
I tried the same settings with timersTIM4and
TIM3 - the result is the same.In the end, it seems that I will haveto include both of the timers from an
external
trigger
.B
ut theproblem will remain unsolved.2013-02-28 11:03 AM
I don't have a 107VC to hand, I used an STM32-VLDiscovery I had to hand, it at least has an F10x family part. I used it as a route to duplicate your issue, and offset.
The behaviour does seem to be undesirable, and not easily explained, may be you can peek the interest of an ST FAE on this one?2013-03-01 10:24 AM
Thank you for the help and interest. I sent an inquiry to ST. If i get a solution from the them, then will write to you.
2013-03-05 1:56 AM
T
ryingto find an answer, I got the answer from Dennis Zheleznyakov(). For that I am very grateful to him!Here
isthe
answer:You use a prescaler ofboth timers, both
prescaler buffer
ized
, ie simply write the value does notchanges, changes occur only after the update events.
Therefore you need to add:
TIM4-> PSC = 70 - 1;
TIM4-> EGR | = TIM_EGR_UG;
This action:
a)
reset bit
b)
set
the newvalue
And everything works as it should!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.