2017-04-19 5:28 AM
Hello,
I'm tring to reset a LED register with a timer (TIM4) interrupt, but TIM4_IRQHandler(void); fucntion it's never launch, the code that i'm using is: (mi board es STM32f429I-DISC1).
Some one can help me please?
Thank you very much for your attention
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////#include 'stm32f4xx.h'TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
void INTTIM_Config(void)
{NVIC_InitTypeDef NVIC_InitStructure;RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);TIM_TimeBaseStructure.TIM_Period = 10 - 1;TIM_TimeBaseStructure.TIM_Prescaler =84 - 1;TIM_TimeBaseStructure.TIM_ClockDivision = 0;TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);TIM_ITConfig(TIM4, TIM_FLAG_Update, ENABLE);TIM_Cmd(TIM4, ENABLE);NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_SetPriority(TIM4_IRQn, NVIC_EncodePriority(4,15,0));NVIC_EnableIRQ(TIM4_IRQn);
NVIC_Init(&NVIC_InitStructure);}
int main(void) {
GPIO_InitTypeDef GPIO_InitDef;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE);
GPIO_InitDef.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14;
GPIO_InitDef.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitDef.GPIO_OType = GPIO_OType_PP;GPIO_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_InitDef.GPIO_Speed = GPIO_Speed_100MHz;//Initialize pinsGPIO_Init(GPIOG, &GPIO_InitDef);GPIO_SetBits(GPIOG, GPIO_Pin_13 | GPIO_Pin_14);INTTIM_Config();
while (1) {
}
}
void TIM4_IRQHandler(void)
{GPIO_ResetBits(GPIOG, GPIO_Pin_13 | GPIO_Pin_14);if (TIM_GetITStatus(TIM4, TIM_FLAG_Update) != RESET)
{TIM_ClearFlag(TIM4, TIM_FLAG_Update);GPIO_ResetBits(GPIOG, GPIO_Pin_13 | GPIO_Pin_14);}}2017-04-19 4:23 PM
did you start the timer ?
in uV5 you can check the peripheral registers on the fly,
you can check if the timer is running.
I start timer 15 above the while(1)
HAL_TIM_Base_Start(&htim15);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.