2013-03-11 2:54 AM
Hi,
I have problems with Timer 8 this time. I want to measure the frequency of an input signal. I have to use PB1 that's connected to TIM8_CH3N
. The code seem correct but it doesn't give any frequency. The code is the following :The main function :int main(void){ /* TIM8 Configuration */ TIM_Config(); TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM8, &TIM_ICInitStructure); TIM_Cmd(TIM8, ENABLE); TIM_ITConfig(TIM8, TIM_IT_CC3, ENABLE); while (1);}void TIM_Config(void){ GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_TIM8); NVIC_InitStructure.NVIC_IRQChannel = TIM8_CC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}The code of the interrupt routine is :
void TIM8_CC_IRQHandler(void){ if(TIM_GetITStatus(TIM8, TIM_IT_CC3) == SET) { TIM_ClearITPendingBit(TIM8, TIM_IT_CC3); if(CaptureNumber == 0) { IC3ReadValue1 = TIM_GetCapture3(TIM8); CaptureNumber = 1; } else if(CaptureNumber == 1) { IC3ReadValue2 = TIM_GetCapture3(TIM8); if (IC3ReadValue2 > IC3ReadValue1) { Capture = (IC3ReadValue2 - IC3ReadValue1); } else if (IC3ReadValue2 < IC3ReadValue1) { Capture = ((0xFFFF - IC3ReadValue1) + IC3ReadValue2); } else { Capture = 0; } TIM8Freq = (uint32_t) SystemCoreClock / Capture; CaptureNumber = 0; } }}Any help to resolve this problem.Thanks.2015-07-10 12:38 PM
2015-07-10 12:59 PM
...when i set 4 MHz frequency, it is showing 8MHz...
I am not interrupting at 4MHz.Really, and HAL_TIM_IC_CaptureCallback() is called by unicorns?You're reading consecutive values of a CCRx register, and measuring the delta ticks between input clock edges.If you were counting pulses, in External Clock mode, you'd sample TIMx->CNT with some periodicity, brief enough that the 16-bit count doesn't overflow. You could latch the value of count into some other TIMx->CCRx register, or via DMA.
2015-07-10 1:01 PM
As I've repeatedly pointed out in this thread, and others, this math is broken
time = ((0xffff - counter)+time);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.