2022-08-05 6:54 PM
I try to setup the PB0 for PWM mode to drive a LED.
When I use the TIM3_CH3, it is working with the following code.
But it does not work for TIM8_CH2N.
I suppose something to do with the "N" but could not find out what in HAL code should be changed.
TIM_OC_InitTypeDef *sConfig;
sConfig->OCMode = TIM_OCMODE_PWM1; // PWM mode 1
sConfig->OCPolarity = TIM_OCPOLARITY_HIGH;
sConfig->OCFastMode = TIM_OCFAST_DISABLE;
sConfig->OCNIdleState = TIM_OCNIDLESTATE_RESET;
sConfig->OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfig->OCIdleState = TIM_OCIDLESTATE_RESET;
sConfig->Pulse = 0;
HAL_TIM_PWM_ConfigChannel(&TimHandle, sConfig, timChannel);
2022-08-05 7:53 PM
> I suppose something to do with the "N"
Maybe. It needs TIMx_CCER.CCxNE to be set. I don't use Cube but it's open source do you can look it up which function sets it. Maybe in the "extended" functions/file.
TIM8 is also an Advanced timer and needs TIMx_BDTR.MOE to be set.
JW
2022-08-06 10:30 AM
Thanks for the hints. Found the HAL code to control it.
when using TIM8_CH2N, need to call the "TIMEx"
HAL_TIMEx_PWMN_Start()
HAL_TIM_PWM_Start()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.