2007-12-16 2:02 AM
TIM4 CCR1 + CCR2
2011-05-17 3:20 AM
Hi,
I want to use TIM4 with CCR1 and CCR2 to generate pulse for two independent stepper motors running att different speed. Everything works as long as not both motors are running at the same time att different speeds. My initialisation sequence: TIM4_ARR = 0xFFFF; TIM4_PSC = PRESCALE - 1; TIM4_CCER &= ~0x1111; // Disable all channels TIM4_CCMR1_OUTPUT_COMPARE_MODE = 0x0000; TIM4_SR = 0; TIM4_CCER |= 0x0011; // Enable channels 1 + 2 Irq_28_to_31_Priority |= 0x00000000; // set priority 0 Irq_0_to_31_Set_Enable |= 0x40000000; // enable irq 30 TIM4_DIER = 0; TIM4_CR1 = 0x0001; // enable TIM4 rewriting registers in the interrupt routine: Motor1 if (((TIM4_SR & 0x0002) != 0x00) && ((TIM4_DIER & 0x0002) != 0x00)){ GPIOC_BSRR = 0x0004; capture1 = TIM4_CCR1; // Update capture register for next edge TIM4_CCR1 = capture1 + motor1.steptime; TIM4_SR &= ~0x0002; GPIOC_BRR = 0x0004; } Motor 2 if (((TIM4_SR & 0x0004) != 0x00) && ((TIM4_DIER & 0x0004) != 0x00)){ GPIOC_BSRR = 0x0020; capture2 = TIM4_CCR2; // Update capture register for next edge TIM4_CCR2 = capture2 + motor2.steptime; TIM4_SR &= ~0x0004; GPIOC_BRR = 0x0020; } With both motors running att different speed there are long pauses in the pulse train. However during short periods of time (ms) both are running as they should. I am puzzled.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.