2012-02-27 1:42 AM
I have the following situation:
- I have a STM32F103RB processor. - Timer 3 configured to generate a PWM signal at the output of PB5. I had to use partial_remap and channel 2 of the timer. Up to this point everything is working properly. - The situation changes if the clock is attached to the I2C1. At this point I have a problem because the output PWM signal PB5 disappears. I do not need no alternate functions for the I2C on this pin. How can I solve this problem? #read-the-errata #tim3-partial-remap-pwm-pb5-i2c12012-02-27 8:17 AM
From the ERRATA document
2.4.8 I2C1 and TIM3_CH2 remapped Conditions �? I2C1 and TIM3 are clocked. �? I/O port pin PB5 is configured as an alternate function output. Description Conflict between the TIM3_CH2 signal and the I2C1 SMBALERT signal, (even if SMBALERT is not used). In these cases the I/O port pin PB5 is set to 1 by default if the I/O alternate function output is selected and I2C1 is clocked. TIM3_CH2 cannot be used in output mode. Workaround To avoid this conflict, TIM3_CH2 can only be used in input mode.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.