2012-03-25 8:23 PM
Hi,
I'm trying to operate the TIM2_CH1_ETR as an external event to clear OCxREF. I have configured:1) PA0 as TIM2_CH1_ETR Alternate function and2) PB11 as TIM2_CH4 PWM output.I'm trying to implement what is described in Section: 13.3.11 and Fig: 99 from the STM32L Manual. The code is as below. I'm not sure what I'm missing, any help on this will be appreciated. TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct; TIM_OCInitTypeDef TIM_OCInitStructure; // Connect TIM2 PWM Output to PB11 pin GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_TIM2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM2); // Enable Timer2 clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE); // Timer2 Configuration TIM_TimeBaseInitStruct.TIM_Prescaler = 0U; TIM_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInitStruct.TIM_Period = 999U; TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseInitStruct); // Output Compare Structure parameters for Duty Cycle TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 450U; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC4Init(TIM2, &TIM_OCInitStructure); TIM_OC4PreloadConfig(TIM2, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM2, ENABLE); // ETR_Initilize TIM_ClearOC4Ref(TIM2, TIM_OCClear_Enable); TIM_SelectOCREFClear(TIM2, TIM_OCReferenceClear_ETRF); TIM_ETRConfig(TIM2, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); TIM_Cmd(TIM2, ENABLE); #etrWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.