2016-05-17 1:58 PM
Hi.
I would like to use PWM input mode on a TIM1. PWM signal on my custom PCB is connected to TIM1 channel 4. Now, I figured out that CubeMX allows to configure PWM input mode only, if PWM signal is connected to channel 1 or 2. Thus, CNT values would be captured in CCR1 and CCR2 registers.I am asking, if it is also possible to connect channel 4 and channel 3 to PWM input mode? Ref. manual doesn't explicitly say that this combination could not be configured. Any idea?Edit: I already found out in other topics that PWM input mode is possible only on CH1 and CH2.Thanks2016-05-17 2:25 PM
No, you'll have to use Input Capture mode and deal with the fact that CNT will not reset. This will involve doing a delta measurement between two subsequent captures, ie B-A
CH4 can act as an alternate input source for CH3We’re moving the ST Community to a new platform to give you a better and more reliable community experience.