2017-01-29 3:29 AM
Hi Forum,
Can anyone tell me why
TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI1, TIM_ICPolarity_Falling, TIM_ICPolarity_Falling);
doesn't work the way I expect it to?
No matter what I tell it to do, it always counts on both edges of the input signal.
I'm using a STM32F103RB with uVision5.22.
Here is the code:
/*-------------------------------------------*/
GPIO_InitTypeDef GPIO_InitStruct;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStruct; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IPU;GPIO_Init(GPIOA, &GPIO_InitStruct); TIM_TimeBaseStruct.TIM_Period = 0xFF;TIM_TimeBaseStruct.TIM_Prescaler = 0;TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStruct); TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI1, TIM_ICPolarity_Falling, TIM_ICPolarity_Falling); TIM2->CNT = 0;TIM_Cmd(TIM2, ENABLE);/*--------------------------------------*/
Thanks,
Wilko
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.