2020-03-02 7:41 AM
2020-03-02 7:53 AM
Hi @ZMa.1
STM32L4 is an MCU not an MPU.
I have change the topic accordingly.
To find example code matching your board refer to STM32CubeProjectsList.html file present in STM32L4 firmware package. ( https://www.st.com/en/embedded-software/stm32cubel4.html )
Hope it help
Olivier
2020-03-02 8:36 AM
@Community member ,
@ZMa.1 might be talking about the Memory Protection Unit in the Cortex-M4 core of STM32L4.
@ZMa.1 ,
The MPU in the Cortex-M3/M4-based mcus is rarely used, so I don't think you'll find many examples. As it's not STM32-specific, you may want to look around and try finding examples also at other Cortex-M3/M4 chips, and/or have a look at Joseph Yiu's "The definitive guide to..." books.
JW
2020-03-02 8:49 AM
Better examples of MPU configuration can be found in F7 and H7 where real cache coherency issues can arise.
Use grep or file manager of choice to search.
/**
* @brief Configure the MPU attributes as Write Through for External SDRAM.
* @note The Base Address is SDRAM_DEVICE_ADDR .
* The Configured Region Size is 32MB because same as SDRAM size.
* @param None
* @retval None
*/
static void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disable the MPU */
HAL_MPU_Disable();
/* Configure the MPU attributes as WT for SDRAM */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = SDRAM_DEVICE_ADDR;
MPU_InitStruct.Size = MPU_REGION_SIZE_32MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
} Same MPU stuff in L4
STM32Cube_FW_L4_V1.14.0\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal_cortex.c
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.