2020-11-04 9:24 AM
Decorated memory store and load for atomic operations
2020-11-04 12:44 PM
There are some families with bit-banded SRAM which allows atomic read/write on bits. Not sure if that's what you're looking for or not.
2020-11-04 3:20 PM
Thanks for reply,
I'm aware of bit banding feature that is only for atomic set and clear operation on single bit from alias address to sigle bit.
I want to know if there is such atomic load and store for "and or xor bit-field-extract bit-field-insert" from decorated address usage, e.g. BME in NXP mcus.
Sorry for my english i hope to be clear
Thanks
2020-11-04 3:54 PM
No.
JW
2020-11-05 2:19 AM
At least GPIO has Bit set and Reset registers for atomic access.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.